Space

Space

Analog Devices is committed to serving the needs of the world space community by manufacturing the highest quality data conversion and signal processing products. Analog Devices’ entry into the space level market occurred in August 1990 when it acquired Precision Monolithics Inc. located in Santa Clara, California. Analog Devices’ certified facilities have been supplying products for military and space applications since 1972. Analog Devices now offers state-of-the-art, data conversion and linear products to the space market place which were previously only available as commercial or military Class B products. Siemens

Analog Devices space level operations located in Greensboro, North Carolina coordinates all Space Level V (Class S) activities, including business development, manufacturing and engineering. The addition of new products is derived from our customers’ needs and the ability of these products to meet MIL-PRF-38535 QML level V requirements.

Analog Devices, Inc. Aerospace Product Line standard product is available in one or more of the following processes:

  • MIL-PRF-38535, QML LEVEL V
  • MIL-PRF-38535, QML D/L/R (LEVEL V with Radiation Qualification)
  • MIL-PRF-38535, JAN S
  • MIL-PRF-38535, Analog Devices, Inc. Standard Space Level Products

New and Featured Products

  • AD9254S: Aerospace 14-Bit 150 MSPS, 1.8V Analog-to-Digital Converter
  • AD8182S: Aerospace Dual 2:1 Buffered, 750 MHz, 3.8 mA, 10 ns Switching Multiplexer
  • AD652S: Aerospace Monolithic Synchronous Voltage-to-Frequency Converter
  • AD8671S: Aerospace Single Precision Very Low Noise, Low Input Bias Current, Operational Amplifier
  • AD8212S: Aerospace High Voltage Current Shunt Monitor
  • AD8351S: Aerospace Low Distortion Fully Differential RF / IF Amplifier
More....

Product Category List

Operational Amplifiers

Analog to Digital Converters

Digital to Analog Converters

Voltage References

Switch and Mux Special Function Products

Radiation Guaranteed List

Analog to Digital Converters
  • AD574S: 12-Bit-ADC w/Microprocessor Interface
  • AD9042S: 12-Bit 41 MSPS ADC
  • AD9058S: 8-Bit Dual 50 MSPS ADC
  • AD6645S: 14-Bit, 80 MSPS Analog to Digital Converter
Comparators Digital-to-Analog Converters
  • DAC08S: Aerospace 8-Bit High Speed Multiplying DAC
  • AD768S: 16-Bit, 30 MSPS Digital to Analog Converter
More....

Generic Radiation Reports

The RADTESTSM DATA SERVICE is a compilation of radiation test results on Analog Devices' Space grade products. It is designed to assist customers in selecting the right product for applications where radiation is a consideration. Many products manufactured by Analog Devices, Inc. have been shown to be radiation tolerant to most tactical radiation environments, Analog Devices , Inc. does not make any claim to maintain or guarantee these levels of radiation toleance without lot qualification test.

It is the responsibility of the Procuring Activity to screen products from Analog Devices, Inc. for compliance to Nuclear Hardness Critical Items (HCI) specifications.

Send Feedback X

Send Feedback

Close